Assumed Confidentiality
The confidentiality of consumers health records is as sensitive as their financial records. People expect the financial institutions they deal with to provide maximum IT security, to protect their financial records, and in the main they do. They also expect healthcare institutions to provide them with the same degree of protection, and in the main they also do. But what happens when you take medical records out of this secure environment and deposit them at the local Pharmacy?
Low Spec meets High Tech
Many independent Pharmacies are little more than a mom and pop store. Technology is often no more advanced than a till and a computer for data records of patients. The more advanced the operation, the more likely they may even have a network closet housing their IT. But isn’t it a risk to have patient confidential files on the same network that any unauthorised check-out operator can access?
Separation Anxiety
In the above scenario, with basic IT know-how, it is not difficult to hack the network to pull data. The dilemma for the Pharmacist is they need access to confidential patient records and the store network without compromising the former.
Separate Networks with Military Grade Technology
This scenario mirrors that of military and intelligence agencies providing access to both classified and unclassified networks. The solution is a secure switch to separate the networks; a switch that guarantees that there can be no contamination from one network to another. So if the patient data is kept on a server separate from the main network and not connected to the internet, security from any hacking or inadvertent data breach is guaranteed.
Large Fines
There are large fines and business reputational issues around breaching patient privacy. Pharmacies can mitigate these risks and potentially reduce their professional indemnity insurance premium by investing in this low cost, simple to deploy and effective IT solution.
Stato di attivazione
Contatta il supporto per i partner Vertiv: NoiPerVoi@vertivco.com
Rivolgiti a un rappresentante di Vertiv che lavorerà al tuo fianco e ti aiuterà a realizzare progetti complessi in base alle tue esigenze. Se la tua organizzazione ha bisogno di assistenza tecnica per un grande progetto, Vertiv può fornirti tutto il supporto necessario.
Molti clienti si affidano ai reseller che sono partner di Vertiv per l’acquisto di prodotti ideali per le loro applicazioni IT. Affidati alle elevate competenze dei nostri partner che, grazie ai prodotti Vertiv, sono in grado di offrire soluzioni complete per infrastrutture e applicazioni IT: dalle specifiche alla vendita all’assistenza.
Sai già di cosa hai bisogno? Vorresti la comodità dell’acquisto e della spedizione online? Alcune categorie di prodotti Vertiv si possono acquistare tramite un reseller online.
Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.
Hai bisogno di aiuto per scegliere un prodotto? Parla con un esperto di Vertiv altamente qualificato che ti orienterà verso la soluzione più adatta.
Impostazioni dei cookie
Facendo click su "Accetta tutto" accetti che sul tuo dispositivo vengano memorizzati i cookie per migliorare la navigazione, analizzare l'utilizzo del sito e contribuire alle nostre attività di marketing.
For more information on which cookies we use, click here.
Drug Store Data Dilemma - Patient Privacy Compromised by Lax IT Security
maggio 04, 2017