Investors

Oracle Solaris for UltraSPARC Release Notes
Network Shutdown Software for Your UPS

By downloading this software you are agreeing to our software license agreement and all terms and conditions of this website.

Oracle Solaris on SPARC Download Instructions/Requirements

  1. Read the operating requirements for this software:
    • SunSoft Solaris on a UltraSPARC processor
    • At least 20 MB of free disk space (during installation, the /tmp directory must have at least 30MB free)
    • Common Desktop Environment or Sun OpenWindows (X Window System)
    • A mouse
    • TCP/IP network protocol
    • Log on to the host as root. You may need to add "execute" mode to the saved file (chmod +x ML_15_xxx_Solaris_SPARC.bin).
  2. Extract the *.bin file from the GNU zip file to a location of your choice and begin the install process
  3. If you intend to connect your Liebert UPS to a serial port on the computer on which MultiLink will be installed, you will need to make or purchase a custom cable for the software to work. ORDINARY SERIAL CABLES WILL NOT WORK! Some UPS models ship with a MultiLink cable. Please refer to the APPENDIX B of the Liebert MultiLink 1.5, Nform Shutdown Client; User Manual (R06/04) (SL-53620) for detailed instruction on "Making Your Own MultiLink UPS Cable" from parts available at most electronics parts stores.

If you decide to purchase a cable instead of building one, you can contact your local Liebert Representative, Value-Added Reseller, or distributor and ask to purchase a MultiLink UPS cable.

Cable for Serial Port Connections

Part No.Description
MLADPT MultiLink Contact Closure Adapter

 

View Downloads for Multilink Automated Shutdown Software

INVESTORS
Overview

Language & Location