Investors

Hewlett Packard HP-UX Release Notes
Network Shutdown Software for Your UPS

By downloading this software you are agreeing to our software license agreement and all terms and conditions of this website.

Hewlett Packard HP-UX Download Instructions/Requirements

  1. Read the operating requirements for this software:
    • HP-UX 11.0 or 11i
    • Appropriate patches applied to operating system. For patches required to run Java 1.4.2, see: http://www.hp.com/products1/unix/java/patches/index.html
    • Common Desktop Environment (X Window System)
    • TCP/IP network protocol
    • 100 MB of free disk space on the partition where MultiLink will be installed (during installation, the /tmp directory must have 200 MB free)
    • A mouse or other pointing device
    • 512 MB of RAM
    • A minimum of 90 threads per process. This is the kernel parameter max_thread_proc, which can be viewed or modified using SAM.
    • HP recommends mid-range N class and low-end L-class systems and PA-8500-based workstations to obtain optimal performance when running Java applications. The recommended minimum system for running Java applications is a PA-RISC 2.0 system or a PA-RISC 1.1 system with a floating-point coprocessor. For information on setting important system parameters required for correct execution of Java programs, go to: http://www.hp.com/go/JAVA
  2. Log on to the host as root. You may need to add "execute" mode to the saved file (chmod +x ML_35_xxx_HP-UX_PA-RISC.bin).
  3. Extract the *.bin file from the GNU zip file to a location of your choice and begin the install process.
  4. If you intend to connect your Liebert UPS to a serial port on the computer on which MultiLink will be installed, you will need to make or purchase a custom cable for the software to work. ORDINARY SERIAL CABLES WILL NOT WORK! Some UPS models ship with a MultiLink cable. Please refer to the APPENDIX B of the Liebert MultiLink Advanced; User Manual; (REV03_08/12) (SL-53625) for detailed instruction on "Making Your Own MultiLink UPS Cable" from parts available at most electronics parts stores.

If you decide to purchase a cable instead of building one, you can contact your local Liebert Representative, Value-Added Reseller, or distributor and ask to purchase a MultiLink UPS cable.

Cable for Serial Port Connections

Part No.DescriptionFunctionUPS Support
MLADPT MultiLink Contact Closure Interface Cable Connects UPS to computer running MultiLink 1.5 or 3.6. Provides On-Battery, Lower-Battery signals only. Liebert UPS models equipped with DB9 ports

MultiLink Part Numbers

Part No.Description
MLADV Liebert MultiLink on CD
MLLKB MultiLink Lincense Kit, 5 Computers
MLLKC MultiLink License Kit, 10 Computers
MLLKD MultiLink License Kit, 20 Computers
MLLKG MultiLink License Kit, 100 Computers
MLLKU MultiLink License Kit, Unrestricted
MLLNA MultiLink Network Administration License

View Downloads for Multilink Automated Shutdown Software

INVESTORS
Overview

Language & Location