Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Updated software enables controlled server shutdown in the event of unexpected power outage

Columbus, Ohio [June 22, 2017] – Vertiv, formerly Emerson Network Power, today released an updated version of Trellis™  Power Insight, a data center management application delivering widespread, centralized monitoring and control of uninterruptible power supply (UPS) systems and networked servers. The solution offers a comprehensive set of alarms, notifications and automated actions, up to and now including controlled server shutdown. The software is included with Liebert® UPS systems. More than 500 users are already using the application, which is available globally.

Trellis Power Insight simplifies management of today’s ever-changing data center environments with auto-discovery of new devices, compatibility and integration with a wide range of Liebert UPS systems, and control through the UPS on-unit, best-in-class touch screen user interface.

“Data centers are increasingly complex, and everything we do is designed to simplify these environments and make management easy and efficient,” said Patrick Quirk, vice president and general manager, global management systems at Vertiv. “With advanced management capabilities, including remote management of distributed IT environments and the ability to safely shut down servers in the event of an outage, Trellis Power Insight  brings peace of mind to data center managers.”

Most data center applications allow for anywhere from 5 to 10 minutes of battery power from UPS units. Trellis Power Insight can monitor up to 50 separate Liebert UPS systems and systematically and safely shut down up to thousands of connected servers in the event of an outage. Controlled server shutdown prevents equipment damage and business interruptions when restarting. 

In addition, Trellis Power Insight provides real-time trending data, including voltage and current, for critical UPS performance. This data is consolidated and viewed in customized dashboards to centralize management of all UPS systems. 

Existing users are able to update their software by visiting the Vertiv software download page on the Vertiv website.

For more information on Trellis Power Insight and other data center power and management solutions from Vertiv, visit www.VertivCo.com.

 

About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.

CONTACT:
Vince McMorrow
T +614 383 1622
Vince.McMorrow@Fahlgren.com

Partner Login

Language & Location