Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for Dutch (EMEA) region.

Vertiv Announces New Suite of Edge Infrastructure Products and Further Develops Award-Winning Partner Programme in Europe, Middle East and Africa

juli 15, 2020

One year after the successful launch of its partner programme, Vertiv adds new benefits for channel resellers and revamps product offerings

Southampton, UK [July 15, 2020] Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, has announced key additions to its award-winning Vertiv™ Partner Programme (VPP) along with an enhanced suite of edge-ready products, including rack power distribution units (rPDU), uninterruptible power supplies (UPS), rack cooling systems, dedicated software and services for partners and customers in Europe, the Middle East and Africa (EMEA).

Following the successful launch of the VPP last year, Vertiv has seen a tenfold increase in its channel partner base across EMEA and is continuing to add benefits for new and existing partners. The brand-new partner relationship management (PRM) system and the enhanced partner portal will enable Vertiv partners to take immediate advantage of tailored trainings to match partner requirements; new sales and marketing tools; online trainings and certification; and product selectors and configurators. The new suite of tools has been designed to help partners develop key skills and knowledge and achieve greater differentiation and profitability along with increased business opportunities.

Joachim Fischer, EMEA channel sales director at Vertiv, said: “We see digitalisation gaining pace and 5G is becoming an ever-closer reality, with more than three-quarters of global telecom operators expecting to be delivering 5G services by 2021. Our enhanced partner programme will continue to equip resellers with the best in class products and services to face the new challenges that technological advances will uncover, such as the critical need for edge deployments. We are committed to the future of the VPP, and, building on an exceptional year, continuing to deliver the highest level of support to allow our channel partners to excel”.

The new suite of products further enhance Vertiv’s comprehensive portfolio of IT technologies and services, tying these into a complete and flexible single-source rack-based solution including:

  • The new Vertiv™ VRC IT Rack Cooling unit with a self-contained and a split version and Vertiv™ Liebert® CRV Row Cooling unit, designed specifically for critical equipment in small server rooms, network closets and edge computing sites. The systems uniquely deploy load-matching, variable-capacity compressors and fans, making these one of the industry’s highest capacity, most efficient cooling units for IT cabinets. The Vertiv VRC is complemented by a complete service package including installation, start-up response time and preventive maintenance.
  • Vertiv™ Geist™ Rack rPDU series with a new 2-in-1 combination outlet for flexible plug connectivity and easy cable management. The Geist™ UPDU is the latest addition to the Geist rPDU family, which features an innovative universal input socket that allows various configurations for customers with multiple deployments across the world. The Geist™ rPDU can access all the devices in the rack to remotely monitor and control these via one single point, monitoring that can be upgraded as technology advances and business needs evolve. The Geist UPDU models enable enhanced performance and management of dynamic IT spaces, while simplifying the buying process and accelerating rapid deployments worldwide. Moreover, the Vertiv Geist rPDU series benefits from the Vertiv™ Distribution Assurance service package.
  • High-efficiency single-phase UPS solutions, such as the Vertiv™ Liebert® GXT5 and the innovative Vertiv™ EDGE line-interactive UPS, which is anticipated to be available on the EMEA channel market by the end of August. In addition, Vertiv’s Lifecycle Power Assurance Services delivers convenient and cost-effective support for power delivery to small IT sites. As edge deployments continue to grow in usage and importance for businesses, Vertiv’s five-year protection plan safeguards small IT sites, providing real-time visibility into critical systems resulting in the early detection of any anomalies.
  • With an anticipated launch in October, the Vertiv™ Avocent® ACS 8000 advanced console server has cellular capabilities, enabling seamless, integrated remote management of Vertiv and third-party equipment, for more efficient and secure network operations even for remote sites or whenever no wired internet is available. Last year Vertiv was ranked by IHS Markit the No. 1 supplier of remote IT management solutions worldwide, a market worth $720m which is continuing to grow strongly together with edge computing and remote IT services.

All of these offerings enable EMEA resellers to earn more points through the Vertiv™ Incentive Programme (VIP), which allows partners to quickly monetise rewards. From July 2020, an enhanced programme known as VIP+ will bring even more benefits to resellers through the silver, gold and platinum level of membership, including lower entry barriers, additional incentives upon registering and higher returns on certain packages. The additions to the scheme will enable even more partners to take advantage of the programme while developing key skills and knowledge at their own pace.

Murtaza Loka, Finance and Purchasing Head at BurhanTec, said: “Working in partnership with Vertiv was already a no brainer due to their world class market position and global end to end product set. This has been enhanced significantly by the Vertiv Partner Program with a range of benefits which has allowed us to take even greater advantage of what Vertiv can offer”.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

CONTACT

Katie Evans
T +44(0)20 3997 8367
E katie.evans@madebychameleon.com

Gerelateerde artikelen

Partner-login

Taal & locatie