The page you're viewing is for Simplified Chinese (China) region.

The page you're viewing is for Simplified Chinese (China) region.

UMIQ-E Configuration

Functionality requires use of Chrome browser


Note: Set "Address" to 0.0.0.0 will enable DHCP. If "Address" is not 0.0.0.0, all other fields must also have valid IP addresses.

If DHCP is enabled ("Address" is 0.0.0.0), "UMG IP" can be 0.0.0.0. In this case, the "Gateway" address in DHCP response will be used as UMG IP.

Download USB driver for Windows 7 here. Install instructions




选择您的本国语言