The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


再販業者を見つける

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Rackmount uninterruptible power supply (UPS) systems and high-density cooling solutions add to portfolio of sustainable edge offerings

Columbus, Ohio [March 29, 2022] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced new power and cooling solutions for the edge of the network, including the Vertiv™ Liebert® GXT5 Lithium-Ion double-conversion, on-line uninterruptible power supply system (UPS). With this news, announced during the Data Center World event in Austin, Texas, Vertiv extends its edge portfolio and adds lithium-ion models to one of the industry’s leading on-line UPS families. The Liebert® GXT5 Lithium-Ion is available for pre-order in the United States and Canada. 

Vertiv also introduced the Vertiv™ Liebert® PSI5 Lithium-Ion Short Depth, a new, shallower configuration of the popular rackmount, line-interactive Liebert® PSI5 UPS system, and two models of the Vertiv™ Liebert® XDU Coolant Distribution Unit, Vertiv’s innovative, drop-in liquid cooling solution for high-density computing environments at core and edge sites. 

“These products share two important characteristics. First, they support the increasingly critical and complex computing environments at the edge of the network,” said Ramesh Menon, vice president of single-phase UPS at Vertiv. “Second, and just as importantly, they support our customers’ sustainability efforts and our pledge to introduce sustainable solutions across the data center ecosystem.” 

The new Liebert GXT5 Lithium-Ion UPS system is Vertiv’s first single-phase online UPS with lithium-ion batteries.

Vertiv leveraged the higher power density of lithium-ion to pack more battery runtime in the same amount of space as a typical valve-regulated lead acid (VRLA) battery. The Liebert GXT5 Lithium-Ion, ranging in sizes from 1kVA to 3kVA, also supports scalable runtime, with a 1U lithium-ion external battery cabinet (EBC). In addition, lithium-ion batteries typically last 8-10 years – roughly the lifespan of the UPS itself – compared to about 3-5 years for VRLA, potentially eliminating costly and inconvenient battery replacements. Lithium-ion batteries are also significantly lighter than VRLA batteries and perform better at higher temperatures, reducing the need for lower temperatures in the rack and by extension, lowering the costs of cooling. 

To meet UL standards, the lithium-ion batteries include an integrated battery management system that monitors the battery at the cell level to ensure safe, efficient operation. The Vertiv™ Liebert® GXT5 Lithium-Ion is compatible with the Vertiv™ Liebert® MicroPOD, an optional maintenance bypass switch that can be installed in the rack behind the UPS, enabling maintenance to the UPS without taking the protected rack equipment offline. 

The Vertiv™ Liebert® PSI5 Lithium-Ion Short Depth is a premium line-interactive UPS packing 3kVA in 3U with a rack depth of less than 16 inches.

This new UPS was designed with two-post racks and wall-mount racks in mind. These racks are common in small spaces at the edge, including retail locations, schools and universities, hospitals, and many telecommunications sites. It features 10 total outlets, compared to just seven for competitive offerings. Like the Liebert GXT5 Lithium-Ion, the Liebert PSI5 Lithium-Ion Short Depth comes with a five-year warranty, standard with all Vertiv™ lithium-ion UPS systems. 

The Vertiv™ Liebert® XDU 450 and 1350 models are extensions of the Liebert® XDU line of Cooling Distribution Units (CDUs), supporting 450 kW and 1.3 MW of cooling, respectively. These systems enable a sustainable adoption of high-density computing in facilities operating with or without water cooling.

Suitable for chip cooling and rear door cooling applications, these CDUs keep the liquid circuit at an elevated temperature and operate at higher temperatures than traditional air-cooled equipment, ejecting heat through the liquid via a dry cooler and ultimately eliminating the need for mechanical cooling or chilled water circuits. The system controller features an intuitive touchscreen that allows for full control of the system, including operator-determined settings and alarm conditions. 

The Liebert PSI5 Lithium-Ion Short Depth is available now in North America. Vertiv is now accepting orders in North America for the Liebert GXT5 Lithium-Ion. The Liebert XDU has models available globally for preorder.  

For more information on the Vertiv™ Liebert® GXT5 Lithium-Ion, Vertiv Liebert® PSI5 Lithium-Ion 3kVA Short Depth, the Vertiv™ Liebert® XDU 450 and 1350, or other Vertiv power and cooling solutions, visit Vertiv.com. For more information on Vertiv’s commitment to sustainability and portfolio of sustainable solutions, visit the Vertiv Sustainability Spotlight.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Sara Steindorf
T +314-982-1725
sara.steindorf@fleishman.com

関連記事

PARTNERS
概要
Partner Login

言語と地域