The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


再販業者を見つける

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Vertiv Introduces New Lithium-Ion UPS
to Support Retail Point-of-Sale, Workstations,
and Other Small Compute Applications in
North America

Vertiv™ Liebert® Power-UPS Lithium designed to provide reliable, economical and long-lasting power protection for critical smaller spaces

Columbus, Ohio [January 11, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced the release of its Vertiv™ Liebert® Power-UPS Lithium uninterruptible power supply (UPS), designed to protect retail point-of-sale (POS) equipment, computers, workstations, wireless networks and routers, surveillance systems and other electronics. The Liebert® Power-UPS Lithium UPS system will be available in Q2 2023 in North America.

The ENERGY STAR certified Liebert Power-UPS Lithium is an efficient, compact and lightweight 400VA/240W 120V UPS system that utilizes lithium-ion battery technology with an 8 to 10 year expected battery life, significantly reducing on-going battery replacements, and providing users with lower cost of ownership. When compared to traditional valve-regulated-lead-acid (VRLA) batteries, lithium-ion batteries have greater power density, last up to three times longer, recharge faster and can endure up to 10 times more discharge cycles. Its flexible design, and a weight of less than four pounds, allows the UPS to be installed in a variety of configurations, making it a convenient solution for environments where space is limited.

“The evolution of remote work, education and small business operations has us relying more on digital equipment and technology to support the essential functions of daily life, which only increases the need to protect these devices from power disruptions,” said Ramesh Menon, vice president, single phase UPS and ITS at Vertiv. “The Liebert Power-UPS Lithium is designed to provide economical and long-lasting power protection that helps maintain uptime and reduce the chance of data corruption by keeping important electronics, including critical retail point-of-sale systems, connected and protected.”

A highly reliable system, the UPS is designed to endure operating temperatures of up to 104 degrees Fahrenheit (40 degrees Celsius) and is ideal for environments with limited airflow and high temperatures. Other features include reliable alarm management, which allows users to quickly identify the problem and to silence the alarm when on battery, and a standard five-year warranty, for added peace of mind that user devices will remain protected and connected.

The Liebert Power-UPS Lithium UPS will be on display in the Vertiv booth at the NRF 2023 in New York, January 15-17. For additional information, visit Vertiv.com.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 24,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

  

CONTACT

Sara Steindorf
T +314-982-1725
E sara.steindorf@fleishman.com

dwad

関連記事

PARTNERS
概要
Partner Login

言語と地域