The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


再販業者を見つける

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

The Energy Star certified Vertiv Liebert PSI5 Lithium-Ion TAA UPS system provides reliable backup power, streamlines procurement for U.S. federal government applications

Columbus, Ohio [March 14, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Liebert® PSI5 Lithium-Ion TAA uninterruptible power supply (UPS) system, the industry’s first and only single-phase lithium-ion UPS system that is fully compliant with the Trade Agreements Act (TAA). U.S. federal government customers who use lithium-ion UPS systems can purchase the system in 1500VA, 1920VA and 3000VA capacities from any qualified Vertiv channel partner in the United States.

TAA compliant equipment is required to be manufactured or substantially transformed in the U.S. or a

TAA designated country, making it acceptable for installation in U.S. federal government facilities as part of a GSA Multiple Award Schedule (MAS) contract where TAA compliant products are required under the contract.

The Liebert® PSI5 Lithium

-Ion TAA is a line-interactive UPS system designed specifically for the edge of the network and distributed IT environments. It delivers up to 20 minutes of battery runtime at half load and 9 minutes at full load – roughly double that of similar capacity UPS systems using traditional valve regulated lead acid (VRLA) batteries. Lithium-ion batteries have greater power density and recharge faster than VRLA batteries, can endure up to 10 times the number of discharge cycles, and last up to 3 times longer than VRLA batteries. The Liebert PSI5 Lithium-Ion TAA comes with a five-year limited warranty with advanced replacement terms, contributing to a total cost of ownership (TCO) that is up to 50% less than VRLA alternatives.

“Lithium-ion batteries have become an important option in data centers of all types and sizes, particularly in the small spaces typical of the edge and U.S. government facilities,” said Tony Evans, vice president, federal strategy and sales, for Vertiv. “The Liebert PSI5 Lithium-Ion TAA provides reliable, sophisticated, long-lasting backup power across their distributed networks, providing an advanced technology that had been lacking for federal agencies and their IT infrastructure.”

The Vertiv™ Liebert® PSI5 Lithium-Ion TAA is Energy Star certified and offers the benefits and functionality of the standard Liebert PSI5, including remote management capabilities and free power management software via optional networking cards.

The Liebert PSI5 Lithium-Ion TAA UPS system is the latest addition to Vertiv’s broad portfolio of TAA-compliant IT infrastructure solutions. Vertiv offers TAA-compliant products across multiple categories, including UPS systems, racks and integrated solutions, rack power distribution, IT management solutions, and thermal management. Other recent additions to the TAA portfolio include the Vertiv™ Liebert® GXT5 double conversion online UPS, and Vertiv® Avocent® ADX Management Platform, including IP and HD KVM devices and a rack manager appliance.

For more information about the Vertiv TAA portfolio and federal government solutions, visit Vertiv.com

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visitVertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Sara Steindorf
T +314-982-1725
E sara.steindorf@fleishman.com

dwad

関連記事

PARTNERS
概要
Partner Login

言語と地域