The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


再販業者を見つける

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Vertiv™ Liebert® GXT5 Lithium-Ion UPS family expands to include 5kVA to 10kVA models for critical edge deployments in North America

COLUMBUS, Ohio [February 7, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Liebert® GXT5 Lithium-Ion double-conversion, on-line uninterruptible power supply (UPS) system for 5kVA-10kVA 120V/208V applications. This expansion of the Liebert GXT5 Lithium-Ion line to 10kVA (from 1-3kVA) further rounds out the Vertiv portfolio of lithium-ion UPS systems and solutions for the edge of the network. Vertiv is now accepting orders for the new 5-10kVA models in the United States and Canada and shipping from current inventories.

The Liebert GXT5 Lithium-Ion models are designed for the smaller spaces typical of the network edge, with a convertible rack/tower design and only a 3U (5kVA/6kVA) or 4U (8kVA/10kVA) footprint. The single-phase input UPS has advanced split-phase output of both 120V and 208V, thus eliminating the need for bulky 208/120V stepdown transformers. An integrated maintenance bypass cabinet preserves additional rack U-space. All Liebert GXT5 Lithium-Ion UPS systems come with a five-year limited warranty.

The higher power density of lithium-ion batteries enabled Vertiv to pack more runtime in less space compared to a typical UPS with valve-regulated lead acid (VRLA) batteries, and that runtime can be extended with up to eight external battery cabinets. With improved performance at higher operating temperatures and longer life expectancy, the lithium-ion batteries in the Liebert GXT5 Lithium-Ion reduce the total cost of ownership by up to 50% compared to VRLA batteries. In addition, lithium-ion batteries typically last eight to 10 years, compared to about three to five years for VRLA batteries, reducing or eliminating the cost and inconvenience of battery replacements during the life of the UPS.   

“We are excited about the Liebert® GXT5 Lithium-Ion launch from Vertiv and the benefits it brings to our customers,” said Mike Parham, technical solutions architect at World Wide Technology (WWT). “With extended runtime, longer battery life and faster recharge compared to VRLA batteries among the improvements, this product will help better protect critical infrastructure and lower support costs.”

“With this expansion of the Liebert GXT5 Lithium-Ion family, Vertiv becomes the first major UPS vendor in North America to offer a full lineup of 1 to 10kVA on-line lithium-ion UPS systems,” said Ramesh Menon, vice president of single-phase UPS and IT systems at Vertiv. “The Liebert GXT5 Lithium-Ion is compact, versatile and low-maintenance – a true set-it-and-forget-it solution ideal for remote locations with limited onsite technical resources.”

Vertiv analysis of IDC data shows that lithium-ion UPS sales revenue in the North American IT channel market grew an incredible 168% in 2022 versus 2021. This greater adoption comes as the industry continues to value the greater power density, improved performance at higher operating temperatures, and longer life of lithium-ion technologies that result in a more environmentally-friendly solution as compared to VRLA battery technologies.

For more information on the Vertiv™ Liebert® GXT5 Lithium-Ion or other Vertiv power and cooling solutions, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statement set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT
Sara Steindorf
E sara.steindorf@fleishman.com

関連記事

PARTNERS
概要
Partner Login

言語と地域