The page you're viewing is for Japanese (Japan) region.

Vertivの製造担当者と連携すると、複雑な設計をお客様独自のニーズに合わせて構成することが可能になります。大規模なプロジェクトに関する技術的ガイドが必要な組織に対して、Vertivは十分なサポートを提供いたします。

詳細を見る

Vertiv再販業者パートナーと連携して、多くのお客様がITアプリケーション用のVertiv製品を購入しています。パートナーは、広範なトレーニングと経験を積み、ITおよびインフラに関するソリューション全体をVertiv製品で明確にし、販売、サポートを行うという独自の立場を構築しています。

再販業者を見つける

ご自身に必要なものについて特定済みですか? 便利なオンラインショッピングおよび配送をご希望ですか? 特定のカテゴリーのVertiv製品は、オンライン再販業者を通じて購入可能です。


再販業者を見つける

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

製品選択にサポートが必要ですか? Vertivの有能なスペシャリストにご相談ください。お客様に最適なソリューションをご提案いたします。



Vertivのスペシャリストに問い合わせる

The page you're viewing is for Japanese (Japan) region.

Flexibility of  Vertiv™ XTE 601E delivers opportunities for reduced costs and equipment footprint

Columbus, Ohio [November 1, 2017]  Vertiv, formerly Emerson Network Power, today introduced the Vertiv XTE 601E, an 84-inch all-in-one outdoor enclosure designed specifically to bring flexibility and a reduced equipment footprint to C-RAN network architectures. Now available to customers in North America, the Vertiv XTE 601E is highly configurable and capable of housing network equipment, DC power and batteries within the same enclosure chamber while tailoring the equipment rack space and a number of battery strings to the needs of the site.
 
That flexibility is critical to C-RAN networks, where electronics traditionally housed at the base of a cell tower can be centralized for use with multiple towers. In turn, this eliminates the need for some enclosures at the cell site, where cellular providers are increasingly seeking options to further reduce equipment footprint and costs.  The Vertiv XTE 601E does just that, allowing providers to house more equipment or more batteries in the enclosure and to adjust that mix as needed. That means the DC power system, battery backup, radio equipment and electronics can be housed in a single, thermally controlled enclosure.
 
C-RAN is a major step forward in cellular network architecture and intelligence, enabling more advanced capacity management, streamlining network operations, and paving the way for 5G,” said Scott Armul, vice president and general manager, DC Power and Outside Plant Products, for Vertiv in the Americas. “Fully leveraging these more intelligent networks requires some fundamental changes to the network infrastructure. The Vertiv XTE 601E delivers the flexibility necessary to make those changes possible and, by reducing the equipment needed to support the network, it helps to reduce capital and operational expenses and service time and costs.”
 
At 84 inches tall, the Vertiv XTE 601E has the capacity to reduce overall cabinet footprint at a site by as much as 75 percent and can support concurrent installation and operation of both macro cell site and C-RAN equipment. That allows cellular providers to make a measured, seamless transition from macro to C-RAN technology.
 
The Vertiv XTE 601E is compatible with either traditional valve-regulated lead acid (VRLA) or nickel-cadmium (NiCad) batteries. Its standard configuration includes two battery boxes, but either or both can be removed and replaced with adjustable rails to accommodate additional equipment. The enclosure is offered with thermal management systems tailored to the environment and the equipment  a heat exchanger in cooler climates or an air conditioner in climates with higher temperatures and/or specific operating needs.
 
For more information on the Vertiv XTE 601E and other communication network solutions from Vertiv, visit www.VertivCo.com.
 
 
About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.
 
Contact
Vince McMorrow
T +614 383 1622
E Vince.McMorrow@Fahlgren.com
PARTNERS
概要
Partner Login

言語と地域