Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv™ Cooling Upgrade Results in Significant Energy Savings for University of Melbourne

March 24, 2017

Sydney, Australia [March 24, 2017] – Vertiv, formerly Emerson Network Power, today revealed that it has supported University of Melbourne’s data centre cooling upgrade, leading to a significant improvement in energy efficiency. 

By installing Liebert® Electrically Commutated (EC) fans to the University’s computer room air conditioning (CRAC) units in place of traditional AC fans, the University was able to reduce its energy use by over 70 percent.

The University of Melbourne is the second oldest university in Australia, and consistently ranked internationally as the top University in the country, as well as among the top 50 worldwide. It engaged Vertiv to assess the potential power savings that could be achieved through modernising its data centre. Tests were conducted before and after the installation of EC fans to do this.

“We expect this to save us more than $2,000 per year,” said Mike Jerrard, operations lead at the University of Melbourne’s IT Department. “Along with cost savings, Vertiv is helping us achieve our 2016-20 Sustainability Plan, which will set pathways for the University's longer term sustainability objectives, including a transition to carbon neutrality by 2030.”

EC fans are more efficient than traditional AC fans as they use permanent magnets instead of a secondary magnetic field in the motor. Because they are electronically controlled, there is no need to waste energy to start the rotor, which leads to better efficiency and performance. 

EC fans also do not require changes to the belt and pulley system – the equivalent of replacing a fan belt in a car. These need to be inspected at least once per year, often leading to a replacement. The process is lengthy and can take half a day or more. EC fans also have a longer service life than conventional AC fans, meaning reductions in maintenance cost and time.

“The University of Melbourne has a huge focus on energy efficiency,” said Robert Linsdell, managing director, Australia and New Zealand, Vertiv. “The renewable energy initiatives and movement away from carbon are testament to that, but the University also recognises that seemingly small changes like this in the data centre can have a major positive impact.”

“Education is an incredibly competitive sector, and taking initiatives like this to reduce costs and carbon footprints can pay huge dividends in staying ahead of the curve,” he added.

To view the full case study, click here.

 

About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centres, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.

CONTACT

Jacqueline Hart
Vertiv
T +612 9805 9510
E jacqueline.hart@vertivco.com

Oisin O’Callaghan
Watterson
T +61 2 9929 7533
E oisin.ocallaghan@watterson.com.au

PARTNERS
Overview
Partner Login

Language & Location