Background
Established in 1853, the University of Melbourne is a public-spirited institution that makes distinctive contributions to society in research, learning and teaching, and engagement. It is ranked among the leading universities in the world with international rankings of world universities consistently placing it as number 1 in Australia and 33 in the world.
| Case Summary | |
|---|---|
| Location: |
Australia |
| Vertiv Solution: |
|
| Critical Needs: |
Melbourne University engaged Vertiv to assess the potential power savings gained with the installation of Liebert™ EC fans. Tests were conducted prior to and after installation of these EC fans to monitor any changes or improvements in the power consumption. |