Sorry, this page isn't available for your location.

The page you're viewing is for Traditional Chinese (Taiwan) region.

Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Sorry, this page isn't available for your location.

The page you're viewing is for Traditional Chinese (Taiwan) region.

Vertiv推出能效一級領先業界氣冷式冰水主機

2021年3月24日

提供節能省錢,又可摒除缺水危機的高CP值空調系統

【台北訊,20210324日】受到極端氣候影響,台灣夏季溫度持續飆高,不僅造成企業對能源使用的需求攀升,也加速環境的惡化。因應這個問題,關鍵數位基礎架構與連續性解決方案全球供應商Vertiv(NYSE:VRT),推出Vertiv模組化氣冷式冰水主機(Vertiv Modular Air-cooled Chillier, Vertiv MACC),協助企業有效節省空間坪數與空調效能。

「據統計,高達40%的企業能源耗損來自於空調,其中,又以冰水主機的耗電量最大,為改善能耗問題,經濟部能源局自2020年7月1日,開始實施冰水主機能源效率分級標示制度(CNS 12575),」Vertiv台灣總經理侯建州表示。「為協助專業技師與企業用戶採購符合能效的產品,Vertiv領先同業推出高於政府要求的一級能效的氣冷式冰水主機,輕巧的模組化設計,讓企業可以靈活安裝、容易擴充與維護,滿足企業的需求。」

 

Vertiv MACC不受台灣缺水危機影響

據業界表示,多數的商用資料中心需耗費30%~70%的能源用量,常利用冷水機或空調來降溫,舉例來說,一般50RT水冷式冰水主機一天開機10小時,水量需求是2.5噸,若冰水主機全天運轉24小時,一天則需要5噸的水量。雖然多數的冷卻系統採取封閉系統,但水塔冷卻也必須補充水,因此,水源枯竭是水冷式系統面對的大挑戰。經濟部水利署表示,去年6月迄今,主要水庫集水區降雨僅約歷年平均值2至6成,台灣正面臨自1964年以來最大的水荒1。水利署進一步強調,因應旱災需要推動緊急抗旱水源計畫,而超前布署的第一要務,即讓全民重視缺水危機、建構節水型社會2。Vertiv模組式氣冷式冰水系統,可以協助力企業摒除缺水危機,利用空氣做為冷卻介質,有效解決並考量使用環境的特性、可用資源、及維護成本。

 

Vertiv MACC五大特色,為業界首選

第一、優於政府認證的能效規定:Vertiv MACC的性能係數(Coeficient of Performance, COP)優於政府一級能效的規定,具備易於安裝、智慧管理與節能安全等優勢,同時,可以降低電費支出。

第二、雙系統獨立的系統架構:Vertiv MACC採用的是全封閉式渦旋變頻壓縮機、雙系統獨立設計、及自動冰水溫度控制機制,可依負載自動調整運轉,實現低能耗、低運行成本的節能省電特點,以及延長壓縮機的平均生命週期。

800x600-Liebert-Modular-Air-Cooled-Chiller

 

第三、易於安裝:Vertiv MACC散熱元件由EC變頻風扇散熱,所以,無需配置冷卻水塔、冷卻水泵及相較於水冷冰機的複雜管路,可輕鬆安裝在任何通風環境,如狹窄的陽台空間或是屋頂角落,支援最多6個單位並排連接,為企業省下至少20%的建置空間。

第四、省電安全:Vertiv MACC支持多機群控功能,通過多台模組化(Teamwork)實現製冷量的增容,及與末端空調的聯動功能。通過與室內空調的聯動實現節能運行,可為多台MACC對單一終端負載進行控制,當氣冷式主機同時開啟並透過變頻壓縮機降載運轉時,性能係數可達4級以上,幾乎趨近於水冷式冰水主機之能效。
 

第五、智慧管理:Vertiv MACC以圖表化視覺介面提供運行資料,內建Modbus及RS485接口搭配後台通訊,即時管理建築設備監控系統(BMS, Building management System)。同時,搭配多種自動保護功能、機房末端聯動功能,及專家級故障診斷系統,極簡化管理維運工作。

未來,Vertiv將透過模組化氣冷式冰水主機,持續優化服務能量,協助台灣企業從空調設備著手、落實「節能高效」的策略目標。

1「驚!台灣其實很缺水 全球排名第18位缺水國家」,葉卉軒,經濟日報,2020年10月30日

2 「蓄水率僅14.9% 民眾車開進曾文水庫底」,黃昱賦、劉漢生,華視,2021年02月19日

 

關於Vertiv 

Vertiv(維諦)致力於保障客戶關鍵應用的持續運行、發揮最優性能、業務需求擴展,並為此提供硬體、軟體、分析和延展服務技術的整體解決方案。Vertiv説明現代資料中心、通信網路、商業和工業設施克服所面臨的艱巨挑戰,提供全面覆蓋雲到網路邊緣的電力、製冷和IT基礎設施解決方案和技術服務組合。Vertiv擁有約2萬員工,在全球130多個國家開展業務。Architects of Continuity™恒久在線,共築未來!如需瞭解更多的資訊,歡迎訪問Vertiv.com

選擇您的國家/區域和語言