Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for Traditional Chinese (Taiwan) region.

高效率的運行模式

2019年7月17日

目前業界最常用的 UPS 拓撲是雙轉換模式;儘管如此,大多數 UPS 設備商已經引入了ECO 運行模式,以進一步提高 UPS 的效率水準。在本文中,我們將分析 ECO 模式操作類型可能的缺點,並進一步強調在使用這些操作模式時應考慮哪些元素。


Vertiv™UPS 為市場引入了新的效率改進方法,已被證明是資料中心的最佳 UPS 解決方案,旨在盡可能降低 PUE,同時保持最高水平的可用性。動態在線模式是 Vertiv 的Liebert®Trinergy™Cube和Liebert EXL S1 兩款 UPS 提供的最新高效操作模式。具有動態在線模式的 UPS 可在不犧牲可靠性的情況下提供高達 99% 的運行效率。實際上,在此模式下,逆變器可以瞬時承擔負載並保持輸出電壓符合 IEC 62040 Class 1 規範。


大型電力供應經理 Valerio ZerilloStephen Major 提出了在沒有負載可用性權衡的情況下實現最高能效的途徑。

下載白皮書

選擇您的國家/區域和語言