Etkinleştirme durumu
Lütfen Vertiv İş Ortağı Desteği ile iletişim kurun: salescloudsupport@vertivco.com
Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.
Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.
Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
Çerez Ayarları
“Tümünü Kabul Et” seçeneğine tıklayarak sitede gezinmenin iyileştirilmesi, site kullanımının analiz edilmesi ve pazarlama çabalarımıza yardımcı olması için çerezlerin cihazınızda depolanmasını kabul etmiş olursunuz.
For more information on which cookies we use, click here.
In addition to tracking battery health, a battery lifecycle management program should enable oversight of the UPS itself. Much like an aging PC or server, the older a UPS system, the greater the risk of failure and the more the UPS will lack in terms of technological innovations and performance enhancements.
With an uninterruptible power supply (UPS), you have made a significant investment in power protection for your operations, so it doesn’t make sense to risk that investment on batteries that may not work when needed most. Your system availability depends on a working battery.
UPS batteries are built to provide several years of service, operating reliably even through repeated charging and occasional use while supporting critical loads. But like any battery, they have a defined lifecycle. The key challenge is to know when your batteries are nearing the end of their life expectancy and to be able to replace them before you get into a situation — such as a complete power outage — where they fail to protect the load.
These smaller UPS systems, ranging in capacity from 500 VA up to 20,000 VA, are usually overseen by IT/network managers and administrators within organizations having edge or remote computing locations. But when it comes to small or remote IT edge installations, out of sight is certainly not out of mind, especially with their vital role in meeting business and customer demands.
In this white paper, we will highlight the critical role of the battery within single-phase UPS systems and discuss the options for ensuring power and business continuity, especially as IT networks increase in size and complexity and/or become more dispersed.
Vertiv, Uç Noktanızı bulmak ve kritik altyapınızı hayata geçirmek için sizinle iş birliği yapar.
Ağ uç noktanız her zaman müşterilerinizin bulunduğu her yere ve ihtiyaç duydukları her şeye yanıt veriyor. Zorluğunuz bu gelişime ayak uydurmak.
Vertiv, Uç Noktanızı bulmak ve kritik altyapınızı hayata geçirmek için sizinle iş birliği yapar.
Ağ uç noktanız her zaman müşterilerinizin bulunduğu her yere ve ihtiyaç duydukları her şeye yanıt veriyor. Zorluğunuz bu gelişime ayak uydurmak.