Współpraca z przedstawicielem Vertiv umożliwia dostosowanie złożonych projektów do indywidualnych potrzeb. Jeśli reprezentujesz organizację, która poszukuje wskazówek technicznych dotyczących dużego projektu, Vertiv zapewni Ci potrzebne wsparcie.

Dowiedz się więcej

Wielu klientów współpracuje z resellerem i/lub partnerem Vertiv, a następnie kupuje produkty Vertiv dla własnych zastosowań IT. Partnerzy są gruntownie przeszkoleni, posiadają odpowiednie doświadczenie oraz są dobrze przygotowani do konfigurowania, oferowania i wspierania rozwiązań oraz infrastruktury IT, przy użyciu produktów Vertiv.

Znajdź resellera

Już wiesz, czego potrzebujesz? Potrzebujesz wygodnych zakupów online i dogodnych warunków transportowych? Niektóre kategorie produktów Vertiv można zakupić za pośrednictwem resellera internetowego.
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
Peak edge performance

Edge is an evolution, not a revolution

Your customers are being asked to meet the ever-increasing demands of their business and downtime is not an option. They need confidence that their infrastructure will stay running well into the future, here are some ways you can help:

 

Downtime Cause Selling Tips: Solutions that can help:
Working with outdated technology

Ensure each critical path is set up with a redundant path so that if one device is turned off or fails, there is another that can step in its place.

Color coding receptacles or power cords to identify A/B feeds can help reduce the chance of accidental removal of cables.

Vertiv Geist rPDU

Vertiv Geist UPDU

Trellis Power Insight

Cyber Attacks You can help by ensuring the hardware purchased is set up with protection as well.

Data Security

Equipment Failure

Ensure proper backup power is purchased in case of a power outage

Liebert GXT5 UPS, 5-20 kVA

Liebert GXT5 UPS, 750-3000 VA

Ensure each critical path is set up with a redundant path so that if one device is turned off or fails, there is another that can step in its place.

Vertiv Geist rPDU

Vertiv Geist UPDU

Outdated equipment can put your customers at a greater risk for failure. Look for programs that help with the transition process.

Trade-In Program

Software Failure

Outdated software is more susceptible to security breaches.

Recommend a new solution that has proper security protocols. Software failure can happen when proper testing has not been done. Recommend to your customer to experiment and test the software before implementing.

Avocent ACS 800

ACS 8000

Avocent Local Rack Access Console

Natural Disasters

If in an area that is earthquake-prone OSHPOD certification is most likely required, Ensure proper backup power is purchased in case of a power outage.

Redundancy is key if your customer’s equipment is located in a high risk area for natural disasters. If possible – recommend setting up geo-redundancy (redundancy between physical locations).

Vertiv VR Rack

Liebert GXT5 UPS, 5-20 kVA

Liebert GXT5 UPS, 750-3000 VA

 

Helpful Talking Points

 

  • Though not every business is the same, a survey showed quarter of companies lose between $301,000-$400,000 per hour of downtime with another 14% losing more than five million dollars per hour.
  • The steep cost of outages not only imposes a direct financial effect, but an indirect operational one as well. The operational strain downtime puts on a business effects added labor and reduced productivity in most cases.
  • There is also an element of reputation loss depending on the company. Take Target’s major data breach in 2013/ That reportedly cost them $162 million, and effected more than 70 million customers, with many of them taking to social media.

Need more information?   Visit our Partner Portal

Dostosuj sieć brzegową klienta dzięki Infrastrukturze Vertiv


Firmy Twoich klientów oczekują, że IT będzie wspierać nowe zastosowania sieci brzegowej i przeniesie moc obliczeniową oraz magazyny danych bliżej klientów, współpracowników i urządzeń. Ale nie są w stanie zrobić tego sami.

Vertiv, Architects of Continuity, dostarcza szeroką ofertę inteligentnych systemów infrastruktury, oprogramowania i usług, które rozwiązują problemy związane z niezawodnością, skalowalnością i zarządzaniem, które pojawiają się wraz z ewolucją sieci brzegowej klientów. Bez względu na wyzwanie, Vertiv posiada odpowiednie rozwiązanie.

Najedź kursorem na każdy wskaźnik na obrazie i kliknij podświetlony obszar, aby uzyskać więcej informacji.

Zarządzanie sprzętem

Dowiedz się, jak ograniczyć przestoje i zwiększyć bezpieczeństwo centrum danych dzięki rozwiązaniom zdalnego dostępu i sterowania Avocent

Konsola szeregowa Avocent ACS 800

Zaawansowany przełącznik konsolowy Avocent ACS 8000

Konsole Avocent Local Rack Access

Przełączniki KVM Avocent MergePoint Unity

Seria przełączników KVM Avocent AutoView

Oprogramowanie do zarządzania Avocent DSView

Szafy i obudowy

Wdrażaj elastyczne oraz ekonomiczne szafy oraz rozwiązania klimatyzacyjne i chroń całe systemy w Twoim centrum danych.

Szafa Vertiv VR Rack

Klimatyzacja precyzyjna

Podstawą zarządzania przepływem powietrza w centrum danych jest rozwiązanie typu korytarz gorąca-korytarz zimna, w których szafy są instalowane w naprzemiennych rzędach, a pobór powietrza przez sprzęt IT (korytarz zimna) usytuowany jest na wprost wylotu powietrza IT (korytarz gorąca). Taka konfiguracja umożliwia operatorom centrum danych kierowanie strumienia powietrza chłodzącego tylko tam, gdzie jest to potrzebne – do miejsc poboru powietrza przez IT – i unikanie zbędnych kosztów oraz strat efektywności wynikających z konieczności chłodzenia całej serwerowni.

Jednostka chłodzenia szafy Vertiv VRC o mocy do 3500 W

Jednostka chłodzenia rzędowego Vertiv CRV o mocy do 33 kW

Zdalne monitorowanie

Niezależnie od tego, czy mówimy o monitorowaniu akumulatora, systemach wykrywania nieszczelności, monitorowaniu temperatury, monitorowaniu przez czujniki w trudnych warunkach przemysłowych, czy złożonych systemach monitorowania centrów danych, wszyscy zgadzamy się, że jest to zasadniczy element przyszłej ochrony i bezpieczeństwa obiektu o znaczeniu krytycznym.

Vertiv Environet Alertjuż wkrótce

Trellis Power Insightjuż wkrótce

Rozdział zasilania w szafie

Linia listew zasilających do montażu w szafie PDU Vertiv spełnia różne wymagania dotyczące rozdziału zasilania w zastosowaniach IT i środowiskowych.​​

Listwa zasilająca Vertiv Geist rPDU

Listwa zasilająca Vertiv Geist UPDU

Zdalny dostęp i sterowanie Szafy i obudowy Chłodzenie szaf rack Zdalne monitorowanie Jednofazowe zasilacze UPS Rozdział zasilania w szafie

Mark Your Calendars

Keep your edge by attending our upcoming events designed for our partners.

 

Powiązane artykuły dotyczące rozwiązań brzegowych

VR Rack Image Alt Text
Case Studies

Infocrossing Manages Its Dynamic Data Centers with Feature-Rich V...

lutego 18, 2020 Dowiedz się więcej
PARTNERZY
Logowanie dla Partnerów

Język i lokalizacja