Współpraca z przedstawicielem Vertiv umożliwia dostosowanie złożonych projektów do indywidualnych potrzeb. Jeśli reprezentujesz organizację, która poszukuje wskazówek technicznych dotyczących dużego projektu, Vertiv zapewni Ci potrzebne wsparcie.

Dowiedz się więcej

Wielu klientów współpracuje z resellerem i/lub partnerem Vertiv, a następnie kupuje produkty Vertiv dla własnych zastosowań IT. Partnerzy są gruntownie przeszkoleni, posiadają odpowiednie doświadczenie oraz są dobrze przygotowani do konfigurowania, oferowania i wspierania rozwiązań oraz infrastruktury IT, przy użyciu produktów Vertiv.

Znajdź resellera

Już wiesz, czego potrzebujesz? Potrzebujesz wygodnych zakupów online i dogodnych warunków transportowych? Niektóre kategorie produktów Vertiv można zakupić za pośrednictwem resellera internetowego.
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
New Thermal Management Solution from Emerson Network Power Minimises Operating Costs for Small Data Centre Rooms

października 05, 2016

Liebert® DCL chilled water rack cooling unit is available in Europe, Middle East and Africa

Southampton, UK [5 October, 2016] – Emerson Network Power, a business of Emerson (NYSE: EMR) and the world’s leading provider of critical infrastructure for information and communications technology systems, today announced the availability of the Liebert® DCL in Europe, Middle East and Africa (EMEA). The Liebert DCL brings a new thermal management solution integrating rack and cooling technologies into one single unit, offering energy efficient water-based cooling that’s intended for small data centre rooms or applications with higher heat densities.

Designed with two different architectures – closed loop and hybrid loop – the Liebert DCL puts chilled water cooling capabilities very close to the heat source. This optimises the amount of air needed for cooling which increases energy efficiency and cost savings. The modular design of the Liebert DCL allows multiple combinations of up to four racks per cooling unit, thus minimizing floor space. Suitable for medium to high heat-load density, the Liebert DCL also reduces power consumption through EC fans and dynamic fan control.

“Considering today’s competitive environment no data centre operator can ignore the issue of costs. After extensive customer research, we have brought to market a cost effective solution that meets current industry requirements and future customer needs,” said Kevin Brady, vice president of Thermal Management for Emerson Network Power in EMEA. “This product is designed for decision makers who want to ensure low running costs over time but still have maximum availability now.”

Availability and efficiency are managed through the integrated iCOM™ Control, which constantly monitors the unit’s supply and return air and adjusts the fan speed to provide the right amount of cold air to the servers. In case of a failure in the control, the unique fail-safe function guarantees continuous operation and maximised cooling by switching the fans to full speed and completely opening the chilled water valve. An additional feature automatically opens the doors of the unit to utilise room cooling as back up. This can be essential in the unlikely event of a system failure or if unacceptable temperatures are reached.

The Liebert DCL is also complemented with sophisticated service capabilities, delivered through Emerson Network Power’s LIFE™ remote diagnostic and preventive monitoring service. From dedicated LIFE centres, Emerson Network Power experts analyse equipment data and trends for proactive maintenance and to recommend actions to ensure the best operational performance.

About Emerson Network Power
Emerson Network Power, a business of Emerson, is the world’s leading provider of critical infrastructure technologies and life cycle services for information and communications technology systems. With an expansive portfolio of intelligent, rapidly deployable hardware and software solutions for power, thermal and infrastructure management, Emerson Network Power enables efficient, highly-available networks. Learn more at www.EmersonNetworkPower.eu.

About Emerson
Emerson (NYSE: EMR), based in St. Louis, Missouri (USA), is a global leader in bringing technology and engineering together to provide innovative solutions for customers in industrial, commercial, and consumer markets around the world. The company is comprised of five business segments: Process Management, Industrial Automation, Network Power, Climate Technologies, and Commercial & Residential Solutions. Sales in fiscal 2015 were $22.3 billion. For more information, visit www.Emerson.com.

Media Contact:
Lara Bunston
+44 208 618 2821
lara.bunston@fhflondon.co.uk

PARTNERZY
Logowanie dla Partnerów

Język i lokalizacja