The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.
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
Vertiv™ VR rack, Vertiv™ Liebert® PSI5 UPS and Vertiv™ rack PDUs expand portfolio of technologies designed to meet demands at the edge in North America

Columbus, OH [August 15, 2018] – Vertiv today introduced power and rack products to meet the unique challenges of the network edge, including the need for rapid deployment, remote monitoring and management, and end-to-end service. These products include the Vertiv™ Liebert® PSI5 uninterruptible power supply (UPS) system, the Vertiv™ VR rack, and Vertiv™ rack power distribution units (rack PDUs) with features to meet the needs of many edge sites. All products will be stocked in North America for quicker availability to help speed deployments.

The launch of these products further expands the Vertiv portfolio of edge solutions. The breadth of product and service choices is critical at the edge, where IT needs may be different from site to site and constantly evolving. A single vendor partner that can provide end-to-end infrastructure solutions and support presents strong value to companies that require edge deployment, but do not have the resources or expertise to sustain this business model.

“As we continue to monitor the evolution of the edge and further define the needs of various edge archetypes, it is clear that one of the key factors for success at the edge is flexibility,” said Angie McMillin, vice president of offering management for Vertiv in the Americas. “With this launch, we add to an edge portfolio that delivers that flexibility by giving our customers options for their edge deployments. By building a broader offering, Vertiv is helping businesses own the edge.”

The Vertiv Liebert PSI5 high performance, line-interactive UPS joins the Vertiv portfolio of rack/tower configurable UPS. This single-phase UPS system is designed for the small spaces and high rack power densities common at the edge. The 2U UPS can be remotely monitored and controlled, has multiple options to meet runtime requirements, and is available with the optional Vertiv Power Assurance Package - a lifecycle support plan that includes installation and startup, on-site service, remote oversight and a 5-year protection plan.

The Vertiv VR rack is a robust and flexible rack solution that allows for rapid deployment. Eight standard sizes are available, all featuring a frame design that delivers about 2.5 inches of additional useable depth compared to similar sized racks, for ease of installation and maintenance of critical equipment. The rack is complemented by a variety of tool-less accessories to help speed deployment and facilitate rack management.

The new Vertiv rack PDUs are available in basic and intelligent models, stocked for rapid delivery. Intelligent models can monitor input power to plus or minus 1 percent accuracy, in addition to standard readings including amps, volts, watts, kWh and power factor. Switched models are available with the ability to monitor and control input power at each outlet, hot swappable modules to allow rapid change in the field, and patented U-lock receptacles that lock any cord in place to eliminate unintentional disconnection are among other notable features. All models have the industry’s best  5 year warranty, when registered within 120 days of purchase, and may also be supported by the Vertiv Distribution Assurance Package lifecycle support, which includes startup, installation, maintenance, repair, emergency response and other features.

To learn more about other Vertiv offerings, please visit www.Vertiv.com.

About Vertiv

Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the Chloride®, Liebert®, NetSure™ and Trellis™ brands. For more information, visit Vertiv.com.

Contact:
Vince McMorrow
614-383-1622
Vince.McMorrow@Fahlgren.com

PARTNERS
개요
파트너 로그인

언어 & 지역