The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.
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
Emerson Network Power Announces Water and Energy Saving Liebert® DSE With Liebert EconoPhase™ Economizer Approved for California Data Centers

9월 16, 2015

Emerson Network Power Announces Water and Energy-Saving Liebert® DSE with Liebert EconoPhase Economizer Approved for California Data Centers

Designed to save millions of gallons of water and increase energy efficiency by up to 50 percent 

Columbus, Ohio [September 16, 2015] – Emerson Network Power, a business of Emerson, (NYSE: EMR) and the world’s leading provider of critical infrastructure for information and communications technology systems, today announced that the California Energy Commission (CEC) has approved the use in California data centers of the Liebert® DSE thermal management system with the Liebert EconoPhase Pumped Refrigerant Economizer. The Liebert DSE system represents a break-through technology that uses no water and saves up to 50 percent of thermal energy, through its patented design and advanced Liebert iCOM controls.

“The Liebert DSE system is a great environmental steward. When used in a typical mid-sized data center of one megawatt load, the Liebert DSE is significantly more efficient than current cooling systems, and eliminate the use of around four million gallons of water each year. If deployed broadly in California data centers, the Liebert DSE with EconoPhase could save hundreds of million gallons of water every year,” said John Peter Valiulis, vice president North America marketing, thermal management, Emerson Network Power.

The CEC has approved theLiebert DSE system with Liebert EconoPhase as a prescriptive economization option, as part of Title 24 of the the CEC’s 2103 Building Energy Efficiency Standards For Residential and Non Residential Buildings, meeting the code’s requirements for energy efficiency and its prescriptive requirements for economizers.

The Liebert DSE system eliminates the need for any water in the heat rejection process and associated chemical water treatment, and it eliminates the risk of exposure to harmful waterbound bacteria. In addition, the Emerson modeling for the CEC compliance program demonstrated an 8 to 10 percent reduction in the data center Time Dependent Valuation measure, compared to the water economizer prescriptive option. The Liebert DSE system design also reduces or eliminates several of the power components associated with water economizers. In actual usage, the entire Liebert DSE system has demonstrated thermal system energy savings of up to 50 percent over older legacy systems.

For more information on Emerson Network Power’s Liebert DSE with EconoPhase or other products and solutions, visit www.VertivCo.com

 

PARTNERS
개요
파트너 로그인

언어 & 지역