The page you're viewing is for Korean (Korea) region.

Vertiv 영업담당자에게 문의하시면 고객의 고유한 요구에 맞게 복잡한 설계를 구성할 수 있습니다. Vertiv는 대규모 프로젝트에 대한 기술 지침이 필요한 조직에 필요한 지원을 제공할 수 있습니다.

자세히 보기

많은 고객이 Vertiv 리셀러 파트너와 협력하여 IT 애플리케이션을 위한 Vertiv 제품을 구매합니다. 파트너는 다양한 교육을 받고 전문 경험을 보유하고 있으며 Vertiv 제품을 통해 전체 IT 및 인프라 솔루션을 지정, 판매, 지원할 수 있는 독보적인 위치에 있습니다.
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
Evaluating Lithium-ion Batteries

Lithium-ion batteries (LIB) are gaining attention as viable replacement for the standard valve-regulated lead-acid (VRLA) batteries, most common as a short term power source with UPS Systems

Frequently Asked Questions

Here are some answers to commonly asked questions about lithium ion batteries in the data centers

Q. What is a lithium-ion battery?
A. Lithium is an alkali metal element; symbol Li on the periodic table. Utilizing Li in the design of a battery provides significant advantages over lead acid.


Q. Lithium-ion batteries are not new, right?
A. Correct. Millions are used every day in our small electronics, laptops, electric cars and more.


Q. Wasn’t Lithium-ion part of the issue with those hover-board fires?
A. True, but those batteries are different chemistries than the ones used in UPS applications which have far more stringent packaging designs. UPS battery solutions have a fail-safe shutdown mechanism which is activated in the event of a problem.

Q. Are there different types of LIBs?
A. Yes. From lithium cobalt oxide (LCO common in small electronics), lithium iron phosphate (LFP), lithium-ion manganese oxide (LMO) and lithium nickel manganese cobalt oxide (NMC) to name a few. Our designers favor LMO and NMC, given their performance and safety parameters. These are the same technologies used by major automotive manufacturers in their electric cars.


Q. Does Vertiv recommend one over the other?
A. Each has differing properties that behave slightly different and may be appropriately used depending on the application.


Q. What are the primary benefits of LIB over lead-acid?
A. LIBs provide impressive power density levels. This means you need less space to deliver the same power. They tend to last longer, weigh less, recharge faster and can operate at higher temperatures.


Q. With such impressive benefits, what are the disadvantages?
A. Predominately initial cost, currently on the order of 1.75x that of VRLA. But a more complete TCO (total cost of ownership) evaluation would include initial cost, installation cost, delayed replacement savings, nuisance value of the replacement, value of space saved, disposal expense and maintenance costs.

Q. Have they been tested in the data center?
A. Though the accumulated runtime in the United States is currently low compared with VRLA, we can answer yes to this question given our experiences in several US installs and in Asia particularly.


Q. Does Vertiv have specific experience with LIBs?
A. Yes. Our engineers and product teams have been on the leading edge of integrating them with UPSs and have fully studied and tested LIBs since 2011. In fact, we have operational customer sites across several continents.


Q. Which of your UPS systems are compatible with LIBs?
A. Much of our midsize and large UPS product lines have been tested and certified for use with lithium-ion battery solutions and are UL approved. See our webpage for more information.


Q. How important is battery monitoring?
A. Very. Fortunately, lithium-ion batteries utilized with UPSs use integrated battery management systems which are part of the UL listing to enhance operation and safety. Additionally, the battery cabinets can be monitored via MODBUS output using traditional monitoring systems.


Q. What is the impact on service and maintenance?
A. LIBs generally require much less maintenance. This saves on operating costs.


Q. What about recycling and disposal issues?
A. Lithium-ion batteries are disposable, but not readily recyclable at this time. As the demand increases, new options are likely to develop. This is not that different than when VRLA's came onto the scene years ago.


Q. Can an installation utilize a hybrid approach, whereby we mix battery technologies?
A. No, if you mean within a unique UPS system. But if more than one UPS system exists, there is no reason you couldn’t operate different type of battery solutions on each.

Download the PDF version of the FAQs or view our UPS Solutions catalog to learn more about how we can help you.

PARTNERS
개요
파트너 로그인

언어 & 지역