Investors

Built to Grow

Partnering to provide infrastructure supporting edge deployments of yesterday, today and tomorrow.

Providing critical infrastructure that evolves with your customer’s edge.

Scalability as it relates to edge deployments can refer to standardizing products and growing across multiple locations or preparing a single location to be able to add equipment in the future. No matter how your customer defines it, here are some tips and ways we can help

 

Their Edge Challenges: Selling Tips: Solutions that can help:

Limited space forexpansion

Maximize usablespace by recommending racks that will fit as much equipment as they can fit.

VRRack – 42U, 45U and 48U

Recommend rack PDUsthat can handle more capacity than is needed today to allow for poweringadditional equipment in the future.

VertivGeist Monitored Rack PDU

VertivGeist Switched Rack PDU

Reduce footprint ofrack-mount equipment where possible to maximize room available for networkequipment.

Vertiv Liebert PSI51U & Mini Tower

Rapidly expandinglocations

Recommend productsthat have a reliable reputation and can be quickly shipped and installed.

VertivVR Rack

Vertiv Liebert GXT5, 500-3000VA

Vertiv Liebert GXT5, 3,000-10,000VA

VertivLiebert PSI5, 750-5,000VA UPS

Vertiv VertivGeist Monitored Rack PDU

VertivGeist Switched Rack PDU

Consider integratedsolutions to take some of the installation headache

Pre-integrated VR Racks

Look for productsthat reduce total cost of ownership (TCO), such as Lithium Ion UPS

Vertiv Liebert PSI5Lithium Ion

Scaling quicklywith limited on-site resources

Find a remotemonitoring & management solution that allows them to not only view databut set alarms and make changes while not physically being there.

Environet

Avocent Serial Console

Avocent IP KVM

 

Helpful Talking Points

 

Find a remote monitoring & management solution that allows them to not only view data but set alarms and make changes while not physically being there.

 

3x

The amount of edge-of-network computing locations that will be required by 2025 to support data proliferation and application sprawl.

One in five respondents expect a

400%

Increase in number of edge sites they will be supporting in the next 5 years.

 

 

Here are some ways your customers are planning for expected growth now:

  • Efficiently adding compute capacity in new locations
  • Choosing site locations strategically
  • Tailoring availability to service requirements
  • Mitigating higher energy consumption with economization
  • Ensuring infrastructure scalability while minimizing capex
  • Enabling remote management

For additional information, Learn More

Recommended Edge Solutions

Offering a comprehensive list of critical infrastructure technologies to help keep your customer’s critical equipment running well into the future.

Select an icon to show solutions

Edge Related Articles

Articles

The Edge of Simplicity

February 08, 2017 Read More
Blog Posts
On the Edge of our Seats
April 04, 2016
Infographics
The Edge Heats Up
October 07, 2016
INVESTORS
Overview

Language & Location