Activation status
Please contact Vertiv Partner Support: salescloudsupport@vertivco.com
Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.
Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.
Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.
Cookies Settings
Technical Cookies
These cookies are essential to ensure the correct functioning of the website, to allow you to register/login and access reserved features, and to allow us to monitor the security of the website and improve operating performance, for example, by storing your preferences to enhance your subsequent visits.
Analytics Cookies
These cookies allow us to collect and analyze traffic and use of the website on an anonymous basis and to understand and improve how visitors use the website, including which pages and products are viewed most frequently. These cookies are not strictly necessary for the website to work but will provide you a better browsing experience.
Profiling Cookies
These cookies allow us to track your navigation of the website to create profiles of your tastes, habits, choices, etc., to send you promotional messages targeted to your preferences. Refusal of these cookies will not affect the proper functioning of the website but will prevent us from being able to send your promotional messages targeted to your preferences.
This website uses cookies
We use cookies to improve your experience on our website. By Continuing, you agree to our use of cookies. For more information, you may view our Cookie Notice and Privacy Policy
- Solutions
- Commercial & Industrial Cooling Solutions
- Indirect/Direct Evaporative Cooling Units
Indirect/Direct Evaporative Cooling Units
Indirect Evaporative Cooling
Indirect evaporative systems perform very well in dry climates with high dry bulb temperatures. Our Indirect Evaporative Cooling Systems are available in many different sizes and configurations and can be customized for any project.
Benefits include:
- Up to 100% outside air supply
- Polymer tube heat exchangers
- Integration with heat recovery systems
- No humidity added to primary air
How It Works
With indirect evaporative cooling, there are two opposing airstreams that contact a different side of a heat exchanger. The outer wall of the heat exchanger contacts air that needs to be conditioned before it is delivered to the occupied space, and the inner wall is in contact with air that comes from the ambient environment or building exhaust.
Indirect evaporative cooling occurs when water sprayed to the interior wall of a heat exchanger evaporates. When the water evaporates, the outer wall of the heat exchanger is subject to evaporative cooling, allowing the airstream to be sensibly cooled.
Direct Evaporative Cooling
Direct evaporative cooling continues to be a popular solution. The process relies on the evaporation of water to produce significant cooling and humidification with minimal energy consumption. Even as technology has progressed, direct evaporative cooling is still the simplest, most cost-effective method of cooling and humidification for air.
Benefits include:
- 100% of evaporative cooling effect felt by room being cooled
- Promotes good air quality by using fresh make up air
- Up to 100% outside air supply
- Quality evaporative media
- Double sloped drain pans
How it Works
Fans force air across an evaporative media, allowing evaporation to occur, resulting in a reduced temperature and increased humidity for the supply air. Wetted media is the substrate needed to allow the most contact of air to the evaporating water, and provides a durable, highly wettable, extended surface with low air-pressure drop. It is self-cleaning and consistent in performance, enabling customers to achieve the full cooling and humidification benefits of water evaporation for the cooled space.