Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (LATAM) region.

What's the Maximum Temperature of Your Server Room?

Server room temperature is one of the most important metrics in any data center environment. Keeping computer equipment at a consistent temperature and humidity point is a critical part of a facility manager's job, and there is a long list of necessary tools that can assist in this endeavor.

That being said, it is incredibly important for data center managers to stay informed of the guidelines they should be following in keeping their facilities in tip-top shape. A disparity of one or two degrees in either direction may not seem like much, but it can make a huge difference in the long run.

What is the maximum temperature a server room can comfortably operate at? What is the minimum? The answers to these questions will give IT managers an idea of the accepted range at which they can keep their facilities.

Baseline standards

The American Society of Heating, Refrigeration and Air-Conditioning Engineers (ASHRAE) is the body that governs the standard for the accepted air temperature and humidity ranges for data center environments. ASHRAE's Technical Committee 9.9 determined in 2011 that a class A1 data center should maintain a temperature between 59 degrees Fahrenheit and 89.6 degrees F, as well as a relative humidity of 20 percent to 80 percent. ASHRAE recommends that facilities should not exceed these guidelines.

Servers should be kept between 89.6 degrees F and 59 degrees F. 

Evolving requirements and possibilities

ASHRAE's guidelines are constantly in flux, having changed in 2004, 2008 and 2011. It helps for data center managers to be well educated and well read when it comes to these changing requirements. For instance, according to Data Center Knowledge contributor Yevgeniy Sverdlik, in 2015, ASHRAE was looking at widening the relative-humidity envelope for data centers to support increased efficiency.

There are some facilities that are taking the temperature beyond the current accepted envelope. For example, Google's Belgium data center operates at a staggering 95 degrees F. This is helping to curb cooling costs and decrease the environmental impact of these huge computing facilities.

Why is this important?

Data center temperature is, as previously mentioned, one of the main metrics for IT managers to watch closely. When equipment temperatures stray outside the accepted ranges, stressful situations can occur.

For instance, when the environment is too warm, overheating can occur, which can result in unexpected server downtime. According to Datacenter Dynamics contributor Penny Jones, this very thing happened to a Microsoft data center in 2013, which caused servers associated with the Outlook and SkyDrive services to experience an unplanned outage.

It is possible for servers to be too cool, as well. While this may not result in any server downtime, data center managers may not want to look at their electricity bill if they're keeping their computing rooms at certain chillier temperatures. The environmental impact of keeping servers this cool is also certainly not negligible. The goal, then, is to keep facilities at the highest temperature possible while at the same time ensuring that servers won't overheat.

Keeping server rooms below the maximum temperature and above the minimum is important for business continuity and efficiency in the long run. Some important questions remain, however: How do managers know their facilities' temperatures at all times? How do they keep temps within the acceptable range uniformly?

Maintaining a strict minimum and maximum server temperature is a critical part of the job of data center managers. By installing an effective cooling management solution offered by Vertiv, facilities can minimize the chance of unplanned downtime and, by the same coin, keep their electricity costs low. Containment solutions can help facilities stay efficient and increase loads without spending extra money on cooling equipment.

Partner Login

Language & Location