Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (India) region.

Vertiv Boosts Range of Industry-Leading Lithium-ion UPS Portfolio in the United States and Canada

March 11, 2021

Vertiv™ Liebert® PSI5 Lithium-Ion single-phase line targets manufacturing, education and edge applications needing long battery life

Columbus, Ohio [March 11, 2021] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today expanded its portfolio of uninterruptible power supply (UPS) systems with lithium-ion battery options through extensions to the120V Liebert® PSI5 lithium-ion line-interactive UPS family. A new 2200VA rack/tower model and the industry’s first 1500VA lithium-ion line-interactive mini-tower configuration join the existing 1500VA and 3000VA rack/tower models. Targeted for edge and distributed IT applications, Liebert PSI5 lithium-ion models are available to order in the United States and Canada through local Vertiv sales offices and value added resellers.

In comparison to valve-regulated lead acid (VRLA) batteries, lithium-ion battery life is up to 2-3x longer, they are rated to function at higher temperatures, are smaller, lighter and deliver longer runtimes. The Liebert PSI5 Lithium-ion family will provide approximately 7-9 minutes of battery backup at full load compared to an estimated 3-5 minutes for a standard UPS with VRLA batteries.

“The benefits of lithium-ion are undeniable and rapid market adoption has pushed prices down to the point that the lifecycle costs clearly favor lithium,” said Jeff Kessen, senior vice president for global product transformation at Vertiv. “We’ve seen adoption increase steadily in the data center, and as more lithium-ion UPS options become available for edge locations, that pattern is repeating.”

The Liebert PSI5 Lithium-ion UPS comes with a five-year warranty on the electronics and battery. It is accompanied by a range of start-up and on-site service options. Vertiv also offers a trade-in program that includes removal, recycling and disposal of old UPS systems when replacing with a Vertiv™ UPS. The rack/tower models are currently available at a promotional price similar to competitive VRLA systems.

In addition to the single-phase Liebert® PSI5, Vertiv offers lithium-ion battery cabinet options for several of its three-phase UPS systems, with capacities supporting up to a 2.4MW load.

Vertiv is introducing the new Liebert PSI5 Lithium-ion models and highlighting its expanding lithium-ion UPS portfolio during the CRN Xchange virtual event in the Vertiv virtual booth. For information on using lithium-ion batteries with single-phase UPS systems, download the Vertiv white paper, The Advantages of Using Lithium-Ion Batteries as A Backup Power Source in Single-Phase UPS Applications for Remote and Edge Data Centers. For more information on the Liebert PSI5 Lithium-ion and other UPS systems from Vertiv, visit Vertiv.com.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

CONTACT

Sara Steindorf
T +314-982-1725
E sara.steindorf@fleishman.com

Related Articles

Partner Login

Language & Location