Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

Vertiv Introduces Pre-Integrated, Micro Data Center Rack Solution for Edge Deployments and Small Spaces in North America

September 16, 2020

Vertiv™ VRC-S integrates rack PDU, cooling and monitoring systems to streamline and simplify installation and setup

Columbus, Ohio [Sept. 16, 2020] – Vertiv, (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ VRC-S, a rack integrated with infrastructure support equipment and designed for fast, easy installation at the edge of the network and other small IT sites. The Vertiv VRC-S incorporates a rack power distribution unit (rPDU), monitoring sensors and software and the new Vertiv™ VRC self-contained rack cooling system in an enclosed, standard-sized IT rack. The Vertiv VRC-S is available now in North America through Vertiv local representatives and numerous distributors and channel partners.

Available in eight pre-built, standard options with two voltage options (120V or 208V), the Vertiv VRC-S streamlines installation and configuration to allow the system to be up and running within hours of delivery. The Vertiv™ Geist™ rPDU provides distribution and switched outlet level control and includes Vertiv™ Intelligence Director software to deliver remote monitoring and management of power and cooling through a single pane of glass.

“Piecing together various IT infrastructure components to meet evolving needs at the edge of the network can be a complex, time-consuming task for today’s IT managers,” said Martin Olsen, vice president of global edge systems for Vertiv. “The new Vertiv VRC-S takes the legwork and wait time out of the equation, offering an integrated, prefabricated data center solution that ships in days and can be installed in hours.”

The integrated, rack-mounted cooling unit in the Vertiv VRC-S is designed specifically for today’s IT loads, and unlike building air conditioning, it does not remove moisture. It delivers 3.5 kW of cooling in a highly efficient closed system that directs cool air to the front of the IT equipment and ejects hot air out the back of the unit and out of the building. The unit’s integrated monitoring system includes sensors at the front and top of the rack that trigger alerts and activate the backup fan for emergency airflow in case of power outages.

The Vertiv™ VRC-S is compatible with Vertiv™ rackmount uninteruptible power supply systems, including the Vertiv™ Liebert® GXT5 UPS. The entire system is available with installation and preventive maintenance services performed by local, factory-trained Vertiv Services professionals.

When purchased as a unit, the Vertiv VRC-S is available with a three-year warranty covering every component of the system. For more information on the Vertiv VRC-S and the full portfolio Vertiv™ thermal management solutions, visit Vertiv.com.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

CONTACT

Schuyler Easterling
T +314-982-8673
E Schuyler.Easterling@fleishman.com

Related Articles

Partner Login

Language & Location