Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find a Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

The page you're viewing is for English (Canada) region.

New system delivers fast, efficient power protection to critical IT edge locations

Columbus, Ohio [Sept. 26, 2017] – Vertiv, formerly Emerson Network Power, today introduced a quick configure and delivery option for the Liebert® EXM UPS system, making it possible to add 10-40 kVA of UPS capacity anywhere in the continental U.S. within four days. The units are highly configurable and address the market’s increasing need for robust computing at the  network edge.

The flexibility of the Liebert EXM quick configure and delivery program extends beyond power capacity. Selections are provided for the output voltage and battery run time to tailor the configuration to a customer’s needs. And in a nod to the increasing criticality across the network, these systems offer a maintenance bypass, allowing service and maintenance to be performed without interruption.

“Today’s network edge is far more than a server in an IT closet,” said Chris Molls, director of AC power sales in North America for Vertiv. “Whether it’s a bank branch or a doctor’s office or any other critical edge environment, they all require robust IT solutions and infrastructure – and they need them quickly. With the Liebert EXM quick configure and delivery bundle, we can deliver enterprise-quality power protection in a matter of days, either directly to the customer or through our channel and electrical partners.”

The Liebert EXM quick configure and delivery bundle also can be configured for 480V operation by adding a transformer in the 30-40 kVA units. The system’s flexibility extends to service plans as well, with packages that include startup and several other options designed to meet the needs of any location or application for fast and simple power deployments.

For more information on the Liebert EXM and other edge solutions from Vertiv, visit www.VertivCo.com.

 About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centers, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.

CONTACT:
Vince McMorrow
T +614 383 1622
Vince.McMorrow@Fahlgren.com

 

Partner Login

Language & Location